Search FAQs
What size breaker is recommended to be used with an HWA, EMA, EBA, & XDSE SPDs.
Product Line:
Surge Protective Devices (SPD's)
Resolution:
EBA & EMA Terminal Torque
![EBA & EMA Terminal Torque EBA & EMA Terminal Torque](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0151H000008zqqiQAA&oid=00DA0000000abSm)
* Note - We recommend a 30 A breaker for installation of these SPD's using #10 wire. If connected to a separate, dedicated branch circuit, the Overcurrent Protection Device (OCPD) setting must be selected to protect the conductors feeding the SPD. Also, when connected to an existing branch circuit, the conductors connected to the SPD must have an ampacity not less than the setting of the existing OCPD.
Surge Protective Devices (SPD's)
Resolution:
- HWA includes #10 AWG wire to be connected to a 30 A breaker in your panel for protection. The EMA and EBA surge protection devices have lugs that are provided for phase (line), neutral, and equipment ground connections.
- The EBA terminals accept a range of 10 AWG (5.26 mm2) to 2/0 AWG (67.4 mm2) copper wire for phase, neutral, and ground connectors.
- The EMA terminals accept a range of 10 AWG (5.26 mm2) to 2/0 AWG (67.4 mm2) with switch offer and 10 AWG (5.26mm2) to 2 AWG (33.6mm2) with NO switch offer copper wire for phase, neutral, and ground conductors.
- The XDSE terminals accept a range of 10 AWG (5.26 mm2) to 8 AWG (8.37mm2) copper wire for phase, neutral, and ground connectors.
EBA & EMA Terminal Torque
* Note - We recommend a 30 A breaker for installation of these SPD's using #10 wire. If connected to a separate, dedicated branch circuit, the Overcurrent Protection Device (OCPD) setting must be selected to protect the conductors feeding the SPD. Also, when connected to an existing branch circuit, the conductors connected to the SPD must have an ampacity not less than the setting of the existing OCPD.
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: