{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is clamping voltage?
Product Line: 
Surge Protective Devices (SPDs)

Environment: 
UL 1449 3rd edition

Resolution:
This is the voltage level at which the surge protection device clips and clamps the voltage at dissipating the overvoltage from damaging the connected downstream devices. The current measurement of clamping voltages is called VPR (voltage protection rating) as referenced in the current UL 1449 3rd edition standards for testing. This is achieved and determined by applying 6000 V and 3000 A to the SPD to obtain the VPR levels.
 

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
move-arrow-top