{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Video: How do you enter the password on the Series 6 IG6 Line Isolation monitor or LIM?
Issue:
Entering the password on the Iso-Gard™ Series 6 IG6 LIM

Product Line:
Line Isolation Monitor (LIM)

Environment:
IG6

Cause:
Programming

Resolution:
Please refer to the video and the attached instructions. The default password is 807. We do not recommend changing the default password. If you lose that password, there is no way to reset the password back to the default. The LIM will need to be replaced.

Schneider Electric Canada

Attachment(s)
How to enter the password for the IG6.pdf [60.22 KB]
Explore more
Category:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Category: