{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Do the 3090TB4/3090TB6 shorting blocks include a cover?
Issue
Customer wants to know if shorting blocks with part number 3090TB4 or 3090TB6 include a cover.

Environment
Wiring, installation

Cause
MySchneider, Digest and the cut sheet for the shorting blocks do not specify if a cover is included.

Resolution
The 3090TB4 and the 3090TB6 do not include a cover.

Note: These were part numbers for shorting blocks that included a cover,
they are now Obsolete

37GP1704SC - 4 pole shorting block w/ cover
37GP1706SC - 6 pole shorting block w/ cover
37GP1708SC - 8 pole shorting block w/ cover

Schneider Electric Canada

Explore more
Category:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Category: