{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What side of an I-Line buss stack can a Surgelogic SPD Unit be installed on?
Product Line:
Surge Protective Devices (SPDs)

Environment:
IMA

Resolution:
The SPD requires 13.5 inches of J frame mounting space.
*Note if used on the wide side three of the 4.5" extensions (HLW4BL) are required. See Surgelogic I-Line Instruction Bulletin for further information.

Schneider Electric Canada

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: