{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Sepam Running Hours Counter is always 0

Issue:
A Sepam relay is reading 0 for Running Hours Counter. This occurs even when I > 0.1IB. SFT2841 and front display will show a non-zero value for Running Hours Counter but it will also be incorrect.

Product Line:
Sepam S20 S24 S40 S42 S80

Environment:
SFT2841

Cause:
Running Hours Counter is a register only available for Generator relays

Resolution:
There are no available registers in the Sepam 20 series of relays for Running Hours Counter.
The only relays with the Running Hours Counter that report correctly are the Sepam G40, G82, G87, and G88

Schneider Electric Canada

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.