Issue:
Determine how much current do the light modules pull.
Product Line:
Harmony 22mm Illuminated Push Buttons
Environment:
Push Buttons and Operator Interface
Resolution:
The current consumption is dependent on the supply voltage.
The information listed in the table below is applicable to all color LED light modules.
Determine how much current do the light modules pull.
Product Line:
Harmony 22mm Illuminated Push Buttons
Environment:
Push Buttons and Operator Interface
Resolution:
The current consumption is dependent on the supply voltage.
The information listed in the table below is applicable to all color LED light modules.
Supply Voltage | Current Consumption |
12 VAC/DC | 18 mA |
24 VAC/DC | 18 mA |
120 VAC | 14 mA |
240 VAC | 14 mA |