Issue:
Availability on epair parts for the HCN series E-1 N3R and N1 enclosures
Product Line:
Panelboards
Environment:
HCN I-line panel
Cause:
Repair parts required
Resolution:
No. there are no longer repair parts available for the series E1 HCN panels for both N1 and N3R. They must replace the panel. There Series E-2 HCN panels are also obsolete so they must replace the entire panel with the new HCM panel. The HCM panel is 32" wide.
Availability on epair parts for the HCN series E-1 N3R and N1 enclosures
Product Line:
Panelboards
Environment:
HCN I-line panel
Cause:
Repair parts required
Resolution:
No. there are no longer repair parts available for the series E1 HCN panels for both N1 and N3R. They must replace the panel. There Series E-2 HCN panels are also obsolete so they must replace the entire panel with the new HCM panel. The HCM panel is 32" wide.