{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

For ground fault alarm on a 5.0P or 5.0H Micrologic trip unit, can a Modbus register be used instead of having to use M2C contacts?

Issue:
Instead of using M2C contacts for GF alarm, what is the correct Modbus register that does the same thing?

Product Line:
Circuit Breakers

Resolution:
Modbus register 8860 can be used for ground fault alarm on 5.0P and 5.0H trip units. It emulates the function of GF alarm in the M2C contacts. Register 8860 changes when both the ground fault pickup level and the time delay level have been met.
(Note: For a register that changes state when only the GF pickup level is exceeded, not waiting for when the time delay to be exceeded, use register 8864).

Schneider Electric Canada

Explore more
Category:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Category: