Issue:
Which guards are compatible with the ZBY9320 legend plate?
Product Line:
Push Buttons and Operator Interface
Environment:
22mm Operators - GIC Product
Cause:
Product Application
Resolution:
No guards are compatible with any of the current line of bezel type 60mm Emergency Stop legend plates. Recommend placing the E-stop in a location where accidental operation is unlikely. This includes the following:
ZBY9320
ZBY9121
ZBY9420
ZBY9220
Which guards are compatible with the ZBY9320 legend plate?
Product Line:
Push Buttons and Operator Interface
Environment:
22mm Operators - GIC Product
Cause:
Product Application
Resolution:
No guards are compatible with any of the current line of bezel type 60mm Emergency Stop legend plates. Recommend placing the E-stop in a location where accidental operation is unlikely. This includes the following:
ZBY9320
ZBY9121
ZBY9420
ZBY9220