{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can a subfeed breaker be added or replaced on a NQO or NQOB Panelboard?
Issue:
Add or replace a subfeed breaker on a NQO Panelboard

Product Line:
Panels

Environment:
NQO and NQOB

Cause:
Addition of a 200A breaker

Resolution:
No, replacement parts are not available for NQO or NQOB panels.
There were no field installed kits available either. Replace the entire panel with the new NQ type.

Schneider Electric Canada

Explore more
Category:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Category: