Issue:
Product Design Features
Product Line:
QO and Homeline load center
Resolution:
Please see below the list of service barrier kits available to meet the UL and NEC requirements:
NOTE: This UL and NEC change became a requirement as of Jan. 1, 2017 and all of the convertible main breaker load centers shipped from the factory will include the service barrier kit. But for all convertible main lug load centers and any backfed applications, the service barrier kit MUST be purchased separately. Also, for all load centers that already exist in the field, the kits MUST be purchased separately.
Product Design Features
Product Line:
QO and Homeline load center
Resolution:
Please see below the list of service barrier kits available to meet the UL and NEC requirements:
Part Number | Description |
---|---|
PKSB1LA | ALL convertible load centers that use QOM1 main breakers |
PKSB1HA | ALL convertible load centers that use QOM2 main breakers |
PKSB1QOBF | ALL QO612, QO816, and QO148... load centers that would use a backfed branch breaker as the main breaker |
PKSB1HOMBF | ALL HOM612 and HOM48.. load centers that would use a backfed branch breaker as the main breaker |
PKSB3 | ALL the 3 phase main breaker load centers |
PKSB3BF | ALL 3 phase load centers that would use a backfed branch breaker as the main breaker |
NOTE: This UL and NEC change became a requirement as of Jan. 1, 2017 and all of the convertible main breaker load centers shipped from the factory will include the service barrier kit. But for all convertible main lug load centers and any backfed applications, the service barrier kit MUST be purchased separately. Also, for all load centers that already exist in the field, the kits MUST be purchased separately.