{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
​Is there an adapter or mounting kit available, to allow a LA36400, LH36400, LDA, LGA, LJA, or LLA 400A breaker to be able to installed on the narrow side of a HCM,HCP,HCW, or HCRU panelboard?
Issue:
Adapter or mounting kit to allow a powerpact or legacy L frame 400A breaker to be able to be installed on the narrow side of an I-line panel

Product Line:
Panelboard

Environment:
I-line panel, HCM, HCP, HCW, HCRU

Cause:
Mounting a branch breaker in an I-line panel larger than 250A on the narrow side.

Resolution:
No. Circuit breakers larger than 250A can only be installed on the wide side of an I-line panel, or on a single row I-line panel like the HCP-SU.

Schneider Electric Canada