Search FAQs
Do NEMA 3R QED-2 and SPEED-D Switchboards come with a sloping roof?
Issue:
Do QED and Speed-D NEMA 3R switchboards come with a sloping roof?
Product Line:
Switchboards built and supported in the USA.
Environment:
Product features
Cause:
Specification
Resolution:
The NEMA 3R roof on the QED-2 and Speed-D switchboards is not sloping.
Do QED and Speed-D NEMA 3R switchboards come with a sloping roof?
Product Line:
Switchboards built and supported in the USA.
Environment:
Product features
Cause:
Specification
Resolution:
The NEMA 3R roof on the QED-2 and Speed-D switchboards is not sloping.
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: