{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What options do we have to use the TeSys T overload on very low amperages?

Issue:
What options do we have to use the TeSys T overload on very low amperages?

Product Line:
TeSys T motor management controller

Environment:
North American Products

Cause:
​Has very low amperage motor and would like to use a TeSys T overload relay

Resolution:

In order to use the LTMR at less than the rated FLC minimum (.4 amps for the LTMR08 devices) we have to loop the wiring through the CT windows on the TeSys T device, and program the multiple passes in either SoMove or the LTMCU.

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: