Issue:
GVAPA2 length
Product Line:
IEC Contactors and Starters
Environment:
TeSys U and GV Motor Starters and Accessories
Cause:
Need to know minimum and maximum shaft length
Resolution:
Our minimum and maximum lengths are 11,9 mm (0.47 in.) to 47,9 mm (1.89 in.)
GVAPA2 length
Product Line:
IEC Contactors and Starters
Environment:
TeSys U and GV Motor Starters and Accessories
Cause:
Need to know minimum and maximum shaft length
Resolution:
Our minimum and maximum lengths are 11,9 mm (0.47 in.) to 47,9 mm (1.89 in.)