Search FAQs
What is the replacement contact kit for 8536 type S starters?
Issue:
What is the replacement contact kit for 8536S series A?
Product Line:
NEMA Type S Full Voltage Contactors and Starters
Environment:
North American Products
Resolution:
What is the replacement contact kit for 8536S series A?
Product Line:
NEMA Type S Full Voltage Contactors and Starters
Environment:
North American Products
Resolution:
Equipment To be Serviced | No. Of Poles in Kit | Class 9998 Parts kit Type No. | |
Type | NEMA size | ||
SA (Series B) | 00 | 3 | SJ1 |
SB | 0 | 3 | SL2 |
4 | SL12 | ||
SC | 1 & 1P | 3 | SL3 |
4 | SL13 | ||
SD | 2 | 3 | SL4 |
4 | SL14 | ||
SE | 3 | 2 | SL6 |
3 | SL7 | ||
SF | 4 | 2 | SL8 |
3 | SL9 | ||
SG | 5 | 2 | SL10 |
3 | SL11 | ||
SH | 6 | 2 | SL25 |
3 | SL26 | ||
SJ | 7 | 2 | SL30 |
3 | SL31 |
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: