{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
UL Listing iEM3000 series and PM3000 series meters
Issue
What is the UL listing for the iEM3xxx Energy meters and PM3xxx power meters

Product Line
iEM3100, iEM3110, iEM3115, iEM3135, iEM3150, iEM3155, iEM3165, iEM3175, iEM3200, iEM3210, iEM3215, iEM3235, iEM3250, iEM3255, iEM3265, iEM3275, iEM3300, iEM3310, iEM3335, iEM3350, iEM3355, iEM3365, iEM3375, iEM3455, iEM3465, iEM3555, iEM3565, iEM3455C1, iEM3455C2, PM3200, PM3210, PM3250, PM3255

Resolution
The iEM3xxx and the PM32xx are listed as Measuring, Testing and Signal-generation Equipment which complies with UL standard 61010 " Safety Requirements for Electrical Equipment for Measurement, Control, and Laboratory Use - Part 2-201: Particular Requirements for Control Equipment" and UL50 "Enclosures for Electrical Equipment, Non-Environmental Considerations" . The UL listing is E360954

Link to UL Listing

Schneider Electric Canada

Attachment(s)
UL Product Spec IEM.pdf [72.43 KB]