Issue:
Establishing bluetooth communication for SR2/SR3 range of Zelio Logic Smart Relay.
Product Line:
Zelio SR2 / SR3 Smart Relays
Resolution:
Bluetooth interface SR2BTC01 and Bluetooth Modbus Adapter VW3A8115 can be used for establishing wireless bluetooth communication between SR2/SR3 Zelio Logic Smart Relay and computer.
Note:
1. The maximum distance between the computer and the module with bluetooth interface is approximately 10 meters.
2. The bluetooth interface SR2BTC01 is compatible with ZelioSoft2 V4.1 and higher.
3. Also it is necessary to have a SR2/SR3 Zelio Logic Smart Relay with a firmware version V4.0 and higher.
The User Manual of Bluetooth interface SR2BTC01 is attached.