{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Video: How does the LK70AN neutral/ground lug install into QO or Homeline load centers?
Issue:
Product Design Features

Product Line:
QO or Homeline Load Centers

Resolution:
The LK70AN branch neutral/ground lug will install on one of the branch neutral bars on the load center interior or can be installed on a PK__GTA ground bar installed in the load center.
The LK70AN will mount under two(2) wire binding screws on the bar and will accept (1) #12 - Al or (1) #14 - 4 Cu wire.

The attached video is ONLY to supplement the INSTRUCTIONS that come with the kit. PLEASE make sure to read the instructions and all the below Safety Information that is located in the instructions BEFORE working on any electrical equipment.

A PDF copy of the complete instructions is attached below the video.

Danger label pic

Make sure to turn OFF ALL Power supplying the equipment and verify the power is OFF using a properly rated voltage sensing device, BEFORE working on or with electrical equipment.
1) Once all Safety steps are followed, begin the kit installation by following the instructions.
2) Remove Cover from load center.
NOTE: When load center is NOT used as Service Equipment neutral assembly is NOT bonded/grounded.
3) Install neutral lug A ONLY in neutral bar B as shown in figures 1 or 2 of the instructions.
NOTE: When load center is used as Service Equipment
4) Neutral Lug A maybe installed in any two neutral bar terminals B.
5) Loosen 2 terminal screws C in neutral bar B and insert both tangs of the neutral lug A into the 2 wire holes of the neutral bar.
6) Position as shown in the instructions and secure with the same two terminal screws to 30 lb-in (3.4 N-m)

NOTE: PLEASE READ ALL INSTRUCTIONS AND SAFETY INFORMATION THAT COME WITH THE KIT AND NEVER WORK ON ENERGIZED EQUIPMENT.

Schneider Electric Canada

Attachment(s)
LK70AN Insert card.pdf [86.66 KB]
Video: How does the LK70AN neutral/ground lug install into QO or Homeline load centers?
Issue:
Product Design Features 
 
Product Line:
QO or Homeline Load Centers
 
Resolution:
The LK70AN branch neutral/ground lug will install on one of the branch neutral bars on the load center interior or can be installed on a PK__GTA ground bar installed in the load center.
The LK70AN will mount under two(2) wire binding screws on the bar and will accept (1) #12 - Al or (1) #14 - 4 Cu wire.

The attached video is ONLY to supplement the INSTRUCTIONS that come with the kit. PLEASE make sure to read the instructions and all the below Safety Information that is located in the instructions BEFORE working on any electrical equipment.

A PDF copy of the complete instructions is attached below the video.

Danger label pic

Make sure to turn OFF ALL Power supplying the equipment and verify the power is OFF using a properly rated voltage sensing device, BEFORE working on or with electrical equipment. 
1) Once all Safety steps are followed, begin the kit installation by following the instructions.
2) Remove Cover from load center.
NOTE: When load center is NOT used as Service Equipment neutral assembly is NOT bonded/grounded.
3) Install neutral lug A ONLY in neutral bar B as shown in figures 1 or 2 of the instructions.
NOTE: When load center is used as Service Equipment
4) Neutral Lug A maybe installed in any two neutral bar terminals B.
5) Loosen 2 terminal screws C in neutral bar B and insert both tangs of the neutral lug A into the 2 wire holes of the neutral bar.
6) Position as shown in the instructions and secure with the same two terminal screws to 30 lb-in (3.4 N-m)

NOTE: PLEASE READ ALL INSTRUCTIONS AND SAFETY INFORMATION THAT COME WITH THE KIT AND NEVER WORK ON ENERGIZED EQUIPMENT.

 

Schneider Electric Canada

Attachment(s)
LK70AN Insert card.pdf [86.66 KB]
Explore more
Range:
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
Explore more
Range:
move-arrow-top