{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Video: How does the LK100AN neutral/ground lug install into a QO or Homeline load center?

Article available in these languages: Spanish

Issue:
Product Design Features

Product Line:
QO or Homeline Load Centers

Resolution:

The LK100AN branch neutral/ground lug will install on one of the branch neutral bars on the load center interior or can be installed on a PK__GTA ground bar installed in the load center.
The LK100AN will mount on the top of the bar by removing the appropriate wiring binding screws pointed out in the instructions with the kit. The LK100AN will accept (1) #6 - 2/0 Al/Cu wire.

The attached video is ONLY to supplement the INSTRUCTIONS that come with the kit. PLEASE make sure to read the instructions and all the below Safety Information that is located in the instructions BEFORE working on any electrical equipment.

A PDF copy of the complete instructions is attached below the video.

Danger label pic

Make sure to turn OFF ALL Power supplying the equipment and verify the power is OFF using a properly rated voltage sensing device, BEFORE working on or with electrical equipment.
1) Once all Safety steps are followed, begin the kit installation by following the instructions.
2) Remove Cover from load center.
3) Remove 3 adjacent wire binding screws A from the appropriate neutral bars as shown in the instructions.
NOTE: In a 1phase and 3phase QO load center, use the inner neutral bars closest to the Main Breaker or Main lugs on the left or right side. In a Homeline load center use the bar on either the Left or Right of the interior.
4) Install neutral lug B ONLY on the neutral bar as shown in the illustrations of the instructions.
5) Secure the neutral lug B with the mounting screw C provided and torque the mounting screw 40 lb-in (4.5 N-m)

NOTE: PLEASE READ ALL INSTRUCTIONS AND SAFETY INFORMATION THAT COME WITH THE KIT AND NEVER WORK ON ENERGIZED EQUIPMENT.

Schneider Electric Canada

Attachment(s)
LK100AN insert card.pdf [75.18 KB]