{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How does the RTC stay on and counting on the M580 when there is a power outage?
Issue:
How long will the RTC be running for when there is a power outage?

Product Line:
M580

Resolution:
Clock Back-Up
The accuracy of the real-time clock is maintained for 4 weeks when the CPU power is turned off if
the temperature is below 45 °C (113 °F). If the temperature is higher, the back-up time is shorter.
The real-time clock back-up does not need any maintenance.
If the back-up power is too low, system bit %S51 is set to 1. This value indicates a loss of time when
the power supply was OFF.

Schneider Electric Canada