{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the Forms to add a TeSys T to a starter?
Issue:
What are the forms to add a TeSys T to a starter? And which TeSys T module is used?

Product Line:
NEMA Type S Starters

Environment:
North American Market

Cause:
Product Selection

Resolution:

The forms, and devices, used are dependent upon NEMA size, full load amperage, and control voltage. Please see the table below for the forms and part numbers.
NEMA SizeRangeCommunication ProtocolFormTeSys T Part Number
Control VoltageControl Voltage
100-240VAC24VDC100-240VAC24VDC
1
.4-8ModbusH612H712LTMR08MFMLTMR08MBD
ProfiBusH613H713LTMR08PFMLTMR08PBD
CANopenH614H714LTMR08CFMLTMR08CBD
DeviceNetH615H715LTMR08DFMLTMR08DBD
Ethernet TCP/IPH616H716LTMR08EFMLTMR08EBD
1.35-27ModbusH622H722LTMR27MFMLTMR28MBD
ProfiBUSH623H723LTMR27PFMLTMR08PBD
CANopenH624H724LTMR27CFMLTMR27CBD
DeviceNetH625H725LTMR27DFMLTMR27DBD
Ethernet TCP/IPH626H726LTMR27EFMLTMR27EBD
2, 35.0-100ModbusH632H732 LTMR100MFM LTMR100MBD
ProfiBusH633H733LTMR100PFMLTMR100PBD
CANopenH634H734LTMR100CFMLTMR100CBD
DeviceNetH635H735LTMR100DFMLTMR100DBD
Ethernet TCP/IPH636H736LTMR100EFMLTMR100EBD
48-160 (CT 300:5 3 turns)ModbusH652H752LTMR08MFMLTMR08MBD
ProfiBusH653H753LTMR08PFMLTMR08PBD
CANopenH654H754LTMR08CFMLTMR08CBD
DeviceNetH655H755LTMR08DFMLTMR08DBD
Ethernet TCP/IPH656H756LTMR08EFMLTMR08EBD
524-480 (CT 300:5 1 turn)ModbusH662H762LTMR08MFMLTMR08MBD
ProfiBusH663H763LTMR08PFMLTMR08PBD
CANopenH664H764LTMR08CFMLTMR08CBD
DeviceNetH665H765LTMR08DFMLTMR08DBD
Ethernet TCP/IPH666H766LTMR08EFMLTMR08EBD
648-960 (CT 600:5 1 turn)*ModbusH672H772LTMR08MFMLTMR08MBD
ProfiBusH673H773LTMR08PFMLTMR08PBD
CANopenH674H774LTMR08CFMLTMR08CBD
DeviceNetH675H775LTMR08DFMLTMR08DBD
Ethernet TCP/IPH676H776LTMR08EFMLTMR08EBD


* NEMA size 6 contactors are only rated up to 810 amps (and should not be used for greater than 810 amps), as such when the contactor rating is programmed in to the TeSys T as 810 amps the device will not let you set a full load amperage over 810 amps.

Note: To order a NEMA starter with a TeSys T motor management controller the product selector should be used.

Schneider Electric Canada