{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What terminal block do I order for the BMXAMI0810?
Issue:
Is there a terminal block available for the BMXAMI0810?

Product Line,
x80 I/O M340 M580

Environment:
These terminal blocks are compatible with the BMXAMI0800 and BMXAMI0810

Resolution:
There are two terminal blocks available for the BMXAMI0810.
BMXFTB2800 (Cage clamp type)
BMXFTB2820 (Spring type)

Schneider Electric Canada

Attachment(s)
X80 Catalogue 2016.pdf [13.81 MB]