{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Are 2-pole and 3-pole EDB breakers available with ground fault protection?

Issue:
Are EDB, EGB, and EJB breakers with GFI protection available in 2 poles and 3 poles versions?

Product Line:
Circuit Breakers

Resolution:
EDB, EGB, and EJB breakers with 30 mA equipment ground fault protection are available in the 1 pole version only (for details, see FA119711).
We do not offer 2-pole and 3-pole E-frame breakers with ground fault protection.

Schneider Electric Canada