{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is ZelioSoft 2 V4.6 Compatible with Tablets?
Issue:
Can ZelioSoft V4.6 be loaded and used on a Tablet?

Product Line:
Programmable Relays - GIC Product

Environment:
US Product

Cause:
Product Application

Resolution:
No, this program is designed for Windows operating systems on a PC platforms.  The system requirements are as shown:
  • PC: Pentium 166MHz (Pentium II 400MHz recommended)
  • Operating system: Microsoft Windows 95,98,2000,XP; NT 4.0 SP5; Internet Explorer 3
  • 64 MB RAM (128 Mb RAM recommended)
  • Free space on hard disk: 60 Mb (150 Mb recommended)
  • 800 x 600VGA screen or higher resolution

Schneider Electric Canada