{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What breakers are available to be DIN rail mounted?
Issue:  
Can breakers be DIN rail mounted?

Product line:  
Circuit Breakers

Resolution:  
The following breakers can be mounted on 35 mm DIN rail as standard:  
  • QOU breakers
  • Multi 9 breakers
  • Powerpact B-frame breaker
The Powerpact H- and J-frame breakers are also DIN rail mountable, but require the S29305 DIN rail mounting kit. The kit is not compatible with 2 pole HD and HG breakers. This kit requires 15 mm depth on a 35 mm DIN rail. See the attached document or visit this link for the instruction bulletin.

Schneider Electric Canada

Attachment(s)
Din Adapter 48940-239-01.pdf [117.99 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
move-arrow-top