{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Are there individual enclosures for the PowerPact B-frame circuit breakers?
Issue:
Product Design Features

Product line:
Molded case circuit breaker enclosures and Heavy Duty Safety Switches

Resolution:
Yes. Below is a list showing the different enclosures that will be available for the PowerPact B-Frame circuit breakers.
NOTE:
These enclosures will ONLY accept 2 and 3 pole B-frame breakers. They will NOT accept 1-pole or 4-pole breakers.

B frame enclosure table

Schneider Electric Canada