{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Can our QED Switchboards (Indoor or Outdoor) be rated for temperature ranges lower than -13F (-25C) or higher than 158F (70 degree C)?
Issue:
QED Switchboards (N1 or N3R) rated for higher temperature ratings than standard

Product Line:
QED Switchboards sold and supported in North America

Environment:
Ambient temperature ratings

Cause:
Operating temperature

Resolution:
No. There is not an option to add cooling units to our switchboards and there are no options for re-rating the breakers to change the operating temperature
ranges of -13F (-25C) and 158F (70C).

If there is a concern of the ambient temperatures and operating temperatures exceeding the above limits, the switchboard should be mounted in air conditioned space.
 

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
move-arrow-top