{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Switch Inside 2510KR1 and 2510KR2
Issue:
What is the part number for the switch only inside the 2510KR2 and 2510KR1?

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
Class 2510 Type K Manual switches

Cause:
Product Characteristics

Resolution:
Yes, the switch inside of the 2510KR* unit can be replaced.
The 2510KR2 uses the 2510KO2.
The 2510KR1 uses the 2510KO1.

Schneider Electric Canada