Issue:
Direct Mount Electronic Overload Relay for LC1D40-LC1D150
Product Line:
IEC Contactors - GIC Product
Environment:
US Product
Cause:
Product Specification
Resolution:
No direct mount units are available above the LC1D38 frame size. A customer can use the LR9D32 with LAD7B205 to mount separate and have an adjustable range of 6.4A-32A. Or the LR9D110S separate mount device which has a range of 22-110 amps
Direct Mount Electronic Overload Relay for LC1D40-LC1D150
Product Line:
IEC Contactors - GIC Product
Environment:
US Product
Cause:
Product Specification
Resolution:
No direct mount units are available above the LC1D38 frame size. A customer can use the LR9D32 with LAD7B205 to mount separate and have an adjustable range of 6.4A-32A. Or the LR9D110S separate mount device which has a range of 22-110 amps