{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
GV2 / GV3 Starter Dial setting
Issue:
Where should the amperage dial be set on a GV2 or GV3 starter

Product Line:
IEC Contactors and starters

Environment:
GV2 and GV3 Manual Motor starters and protectors


Cause:
Installation and Setup

Resolution:

These overloads take into account a standard 1.15-1.25 service factor, and the trip setting is 125% FLA.  For motors with these service factors the amp dial should be set as close to the motor nameplate full load current as possible.
Outside of this range we recommend reaching out to the motor manufacturer for a recommended multiplier.

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: