{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the correct way to store a Motor Control Center before installation?

Issue:
Storage conditions of Model 6 MCC

Product Line:
Products sold in North America

Resolution:
If the MCC cannot be placed into service upon receipt, store it in a clean, dry, ventilated building free from temperature extremes.  Acceptable storage temperatures are from
0 degree C (32 degree F) to 40 degree C (104 degree F).  Acceptable humidity levels are 0 to 95%, non-condensing.

If the storage area is cool and/or damp, provide enough heat to prevent condensation inside the MCC.
Note; failure to comply with these recommendations can void the warranty on the product.

Schneider Electric Canada