{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What overcurrent protection is required on the SDSA1175 or SDSA1175T Surge Protection device?

Issue:
What overcurrent protection to use on the SDSA1175 or SDSA1175T surge protection device?

Product Line:
Surge Protection Devices, SPD

Environment:
SDSA

Cause:
Breaker specification to protect equipment

Resolution:
The SDSA1175/SDSA1175T comes with #14 wire.  You can connect it three different ways.
1) You can connect to a existing breaker feeding another load if lug terminals will accommodate multiple conductors.
2) You can connect to a dedicated 20A breaker.
3)  You can direct bus connect because it is a Type 1 device. Type 1 SPD can be connected with or without an overcurrent protection device.

To reach a Surge Protection Specialist direct please call 800-577-7353 or email: spdtag@schneider-electric.com

Schneider Electric Canada

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range: