Search FAQs
Are circuit breakers horsepower or motor rated?
Issue:
Are breakers hp rated?
Product Line:
Miniature, Molded Case and Air Circuit Breakers
Resolution:
Circuit breakers are not HP or motor rated. Breakers are chosen based upon the NEC requirements and the protection required for the motor.
Are breakers hp rated?
Product Line:
Miniature, Molded Case and Air Circuit Breakers
Resolution:
Circuit breakers are not HP or motor rated. Breakers are chosen based upon the NEC requirements and the protection required for the motor.
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: