{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the highest ampacity Powerpact R-frame breaker that can be installed as an individually mounted main breaker in a QED-2 switchboard?

Issue:
Why can't I install a 3000 A R-frame breaker in my QED-2 switchboard?

Product line:
Main breaker switchboard sections

Environment:
QED-2 switchboards with main breakers

Resolutions:
The highest ampere R-frame that will install in a main section of a QED-2 switchboard is 2500 A.  If 3000 A or higher is needed, you must use a Masterpact NW.

Schneider Electric Canada