{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is the Size 00 Nema starter available in a Nema 7/9 hazardous duty enclosure?
Issue:
Checking if the Size 00 Nema starter is available in a Nema 7 or 9 hazardous duty enclosure

Product Line:
NEMA Contactors and Starters

Environment:
8536 Type S NEMA Starters

Cause:
Selection/application

Resolution:
No, customer must select Size 0 to obtain a Nema 7/9 hazardous duty enclosure.  It is not available in Size 00.



Schneider Electric Canada