{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Video: How to install a second shunt trip or undervoltage trip on motor operated a PowerPacT P frame
Issue:
How do you install a second shunt trip or an undervoltage trip/release on an electrically operated PowerPacT P-Frame circuit breaker?

Product Line:
Molded Case Circuit Breakers

Resolution:
Remove the 4 screws on the sides of the breaker and remove the cover. Remove the triangular hold down piece on the top of the breaker. Slide the shunt trip or undervoltage trip with the flat piece facing the trip unit and the wires facing towards the opposite side of the breaker. Slide the connection piece into place with the screws facing upward. Then plug the connecting wires from the shunt or undervoltage into the connection piece. Then place the triangular hold down piece back into place, matching the orientation that it was originally installed in. See below video or attached instruction bulletin for more information:

Schneider Electric Canada

Attachment(s)
M, P, R Frame Shunts and Undervoltages.pdf [1.49 MB]