{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is there a SCCR rating for the LC1F1700 and LC1F2100 contactors?
Issue:
SCCR for LC1F1700 and LC1F2100 contactors

Product Line:
IEC Contactors - GIC Product

Environment:
US Product

Cause:
Product Specifications

Resolution:
The LC1F1700 and 2100 are not “UL listed” devices but are UL standard compliant, duly confirmed by an NRTL recognized organization. (NRTL : Nationally Recognized Testing Laboratory). According with the applied UL 60947-4-1, due to the fact they are not intended for motor control and have no hp ratings, no short-circuit tests were required.

Schneider Electric Canada