{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What's the maximum FLA on a TeSys T LTMR?

Issue:
What can limit the maximum FLA of the TeSys T overload relay?

Product Line:
TeSys T Motor Management Controller

Environment:
Products Sold in North America

Cause:
Installation and Programming


Resolution:
There are three sizes of TeSys T overload relay, the LTMR08, LTMR27, and LTMR100.
The devices have the ranges below without external CTs and with no modifications made in the programming:
LTMR08.4-8 amps
LTMR271.35-27 amps
LTMR1005-100 amps

This means that with no modification of settings or addition of external CTs these devices will have a maximum FLA of 8, 27, and 100 amps respectively.
If you add external CTs, and program this via SoMove or the HMI, the maximum and minimum FLA value can increase. If you have your wire pass through the internal CT window of the device multiple times, and program this via SoMove or the HMI, your FLA min and max values will decrease.

But those aren't the only parameters that will affect the FLA range of your TeSys T. The "Contactor Rating" will also affect the range, and if the contactor rating is lower than the default maximum of the device, or even lower than the range would be with CTs, this will be your new maximum FLA.
For example if you have an LTMR08 with 300:5 external CTs and one pass through the internal CT window  your LTMR FLA range should be 24-480 amps. If you have this device on the output of a NEMA size 4 starter though your contactor rating should be programmed to 135 amps, due to this your overload range will still have a minimum of 24 amps but the maximum value will now be 135 amps.

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: