{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What versions of PME are supported with the Configuration Manager tool?
Product Line
Configuration Manager tool

Environment
Supported PME versions

Resolution
*The use of this component, and any component in the Toolkit, has the potential to modify system configuration and should only be used by competent personnel. Backups of database and/or System Configurations should always be made prior to utilizing tools. Schneider Electric bears no responsibility for changes made as a result of the use of this tool. The component is posted on an as-is basis.*

The most recent version of the Configuration Manager Tool, as well as previous versions, can be found in FA316723, which contains links to articles that discusses which versions of PME are supported for each version.

Schneider Electric Canada

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: