{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What can be done when the error "LTU does not work with the micrologic demonstration unit" shows on the LTU software?

Issue:
When I try to test a breaker with the LTU, I get the error "LTU does not work with the micrologic demonstration unit"

Product Line:
Molded Case Circuit Breakers

Resolution:
This may happen when an older version is being used on Windows 7. To fix the error, update to the latest version using this link. Also, make sure to use the 32 bit version, regardless of computer: https://www.se.com/ww/en/download/document/LTU_Test_Software/

Schneider Electric Canada