{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Video: How does bit to word conversion work in Zelio Soft 2?
Issue:
How to understand Bit to Word conversion function block in Zelio Soft 2 for Zelio Smart Relay

Product Line:
Zelio Smart Relay SR3NET01BD

Environment:
North American Products

Cause:
How to understand Bit to Word conversion function block in Zeliosoft 2 for Zelio smart relay

Resolution:
Make sure the SR3NET01 module is added in the Zelio Soft 2 program.
An SR3NET01BD Ethernet extension may be added to SR3B261BD, SR3B262BD, SR3B101BD and SR3B102BD smart relays.
In FBD mode, if the extension is present, then the application can use the four contacts J1 to J4 as inputs and the four contacts O1 to O4 as outputs. Each contact represents a 16-bit Modbus word.
The Ethernet extension exchanges Modbus messages as a server and by using the suite of TCP/IP protocols and Ethernet technology.
The Ethernet extension has four 16-bit inputs:
J1 (address 16),
J2 (17),
J3 (18),
J4 (19).
These words may be accessed in read and write modes.
Ethernet Outputs
The Ethernet extension has four 16-bit outputs:
O1 (address 20)
O2 (21),
O3 (22),
O4 (23).
These words may be accessed in read mode only.
A sample demo program has been created in the video below to demonstrate how the Bit to Word conversion function works.

Schneider Electric Canada