{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Video: How to install unit mount PowerPacT B-frame onto back pan
Issue:
How do you install the unit mount PowerPacT B frame breaker onto a back pan?

Product Line:
Molded Case Circuit Breakers

Resolution:
First, you will remove the green connection system covers. Make sure to line up the breaker with the mounting holes, and then use two diagonal slots near the lugs to install the mounting screws into. Once they are tightened to the proper torque, reinstall the green connection system covers. For more information, see the instructional video below:

Schneider Electric Canada