{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Covers for 30mm Emergency Stop Buttons
Issue:
Are there any clear covers available for 30mm E-stop buttons?

Product Line:
Push Buttons and Operator Interface

Environment:
30 mm Emergency operators

Cause:
Product Accessories

Resolution:
Clear full covers enclose the E-Stop entirely in a clear case, and we do not want to hinder access to our operators as they are typically utilized in industrial applications.  As such, we do not offer a full clear cover for these operators.

Schneider Electric Canada