{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Video: How to replace a Micrologic trip unit on a PowerPacT™ P frame, R frame, or Masterpact NT or NW breaker

Issue:
How to replace a Micrologic trip unit on a PowerPacT™ P-frame, R-frame, or Masterpact NT or NW Breaker

Product Line:
Molded Case Circuit Breakers

Resolution:
NOTE: The ET1.0I trip units are NOT replaceable. Only the Micrologic trip units (3.0, 5.0, 3.0A, 5.0A, 6.0A, 5.0P, 6.0P, 5.0H, and 6.0H) are replaceable. Also, note that if you are replacing a 3.0 or 5.0 trip unit with an ammeter, power, or harmonic trip unit, you will also need to order the green 12-pin connector (kit S33101 for Masterpact, S33100 for PowerPacT™).

First, remove the accessory cover. After doing so, remove the 12-pin connector (if one is installed) on the top of the trip unit. Then loosen the top and bottom screws of the trip unit, and slide it out. Slide the new/replacement trip unit back in its place, and re-tighten the screws. Reinstall or install the new 12-pin connector (if needed). For more information, see the attached instruction bulletin or the instructional video below:

Schneider Electric Canada

Attachment(s)

P, R Frame, Masterpact Trip Unit Replacement.pdfP, R Frame, Masterpact Trip Unit Replacement.pdf [557.76 KB]