{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is it possible to order PM5500 mounting clips separately?
Issue
A customer would like to purchase the PM5500 mounting clips separately.

Product Line
Powerlogic PM5500

Environment
Installation - Mounting Clips

Cause
A customer has broken or misplaced the mounting clips for a PM5500 meter (integrated or remote display).

Resolution
Unfortunately, the mounting clips cannot be purchased separately. They can, however, be purchased as part of the mounting hardware kit.

Part numbers for the two models are the following:
- METSEPM55HK for integrated display model (PM5560)
- METSEPM55HKRD for remote display model (PM5563RD)

Schneider Electric Canada