{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the part number for an upper 12 in horizontal wireway cover for the Model 5 and Model 6 MCC's?
Issue:
Identify a part number for an upper horizontal wireway cover for Model 5 and Model 6 MCC

Product Line:
Model 6 Motor Control Center

Environment:
Motor Control Center Spare Parts Model 6

Cause:
Replacement Parts

Resolution:
The 12in x 20in upper horizontal wireway cover for a Model 6 Motor Control Center is part number 80450-140-50.

Schneider Electric Canada