{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Is there a Class 9422 Variable-Depth Operating Mechanism for the Powerpact M / Powerpact P Frame breakers?

Issue:
Need to find a variable depth operating mechanism for Powerpact M/P breakers.

Product Line:
Variable-Depth Operating Mechanism

Environment:
US Product Lines

Cause:
Product Selection

Resolution:

The catalog number is 9422RM1, this does not have the 9422 handle operator. For handle operator use Type AP1, AP2, AP9, or AP10 operating handles.

All circuit breaker operating mechanisms are suitable for either right- or left-hand
flange mounting, convertible on the job.

Variable mounting depth range: 10.50-18.38 inches

Drawing: http://static.schneider-electric.us/docs/Circuit%20Protection/Operating%20Mechanisms%20and%20Disconnect%20Switches/9422_RM_OUTLINE_001.pdf

Instruction Bulletin : http://download.schneider-electric.com/files?p_enDocType=Instruction+sheet&p_File_Id=4135951900&p_File_Name=30072-452-42_01.pdf&p_Reference=30072-452-42

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: