{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Do the J frame circuit breakers come with both wire binding screws (long and short)?
Issue:
Need to know if the longer and shorter wire binding screws are both provided with J-frame circuit breakers

Product Line:
Molded Case Circuit Breakers

Resolution:
The electronic trip J frame circuit breakers come with the AL250JD lug kit, as well as the alternate longer wire binding screw. The thermal magnetic J frame breakers rated 150 and 175 A come with the AL175JD lug kit and no alternate wire binding screw. The thermal magnetic J frame breakers rated 200, 225, and 250 A come with the AL250JD lug kit and no alternate wire binding screw.

Schneider Electric Canada